CAP#.PREEDGE

Description

If precondition mode 1 has been selected, then this selects which edge of the precondition input will be waited for before the trigger is allowed.

Examples

Usage

1: Rising edge (default)

2: Falling edge

3: Rising or falling edge

Code

-->CAP1.EDGE 1
-->

Context

For more information please refer to Capture.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

1 to 3

Default Value

1

Data Type

Integer

See Also CAP#.PREMODE, CAP#.PRESELECT
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
CAP1.PREEDGE

4400h

02h

Unsigned8

-

-

Read/Write

No

CAP2.PREEDGE

4401h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

CAP1.PREEDGE

31040

7940

Unsigned8

Read/Write

-

CAP2.PREEDGE

31041

7941

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

CAP1.PREEDGE

31040

Unsigned8

Read/Write

-

CAP2.PREEDGE

31041

Unsigned8

Read/Write

-

Related Topics

Capture

CAP#.EDGE